Digital Inputs and Outputs

The drive has programmable digital inputs and outputs that you can use to initiate motion, control auxiliary devices, or trigger other actions. The inputs and outputs should be wired according to the instructions in the drive Installation Manual (I/O Connection (X21/X22/X23)).

Using Digital I/O

Once wired correctly, digital inputs and outputs can be used for a variety of functions, such as to trigger auxiliary devices, initiate homing moves or other motion tasks, or set travel limits. I/O settings are configured on the Digital I/O WorkBench page. The I/O signal is only used when activated by the desired function.


  • When using I/O devices, you must carefully consider the type of device you use for switches. An unsuitable switch can cause switch bounce, which in turn can cause erroneous triggers to occur. For example a low cost xx switch, as it is toggled, will bounce a few times before it turns on or off. A device that is monitoring these inputs frequently may interpret the bounce as multiple triggers of that I/O. The drive has the ability to reduce this type of error using some debounce techniques to ignore sudden state changes caused by bounces.

Digital Inputs

Digital inputs can be used as a source for a number of drive functions (Action Table, limit switches, homing, etc). The input becomes active depending on the polarity setting and the wiring setup. Default behavior is the input becomes active (DIN#.STATE = 1) when 24V is applied to the IO pin (active high). If polarity is set to active low, the input state becomes active when voltage is removed on the IO pin and becomes low when 24V is applied. An additional signal filter can be configured on each IO pin to filter out glitches.

Element Description Parameter
Polarity

Set when the input state becomes active, when the polarity is High or Low.

  1. Active High
  2. Active Low
DIN#.INV
Filter

Setting a filter blocks input changes from registering until the specified pulse width is exceeded.

  1. Off (unfiltered)
  2. 10µs (fast)
  3. 163µs (standard)
  4. 2.62ms (slow)
  5. 240ns (ultra fast)
DIN#.FILTER
Alert An alert sound can be played through the PC when the state changes.  
LED icon This LED displays the state of the input, green for Active, off for Inactive. DIN#.STATE

Digital Outputs

Digital outputs can be driven manually with DOUT#.STATEU or as an indication driven by another module. The behavior of each digital output is controlled based on DOUT#.SOURCE. When activated, the digital output will provide 24V on the IO pin.

Element Description Parameter
Source

Set the source of the digital output.

  1. User - the output value is controlled by the user. The On/Off switch enables/disables DOUT#.STATEU
  2. Action Table - the output value is controlled through the Action Table.
  3. FieldbusClosedA Fieldbus is an industrial network system for real-time distributed control (e.g. CAN or Profibus). It is a way of connecting instruments in a plant design - the output value is controlled by the fieldbus (3601h Digital output control) Digital Output Control)
DOUT#.SOURCE
Source ID Sets the source ID of the selected source when required. In some cases, the source could have several instances and the user has to select which one to use. DOUT#.SOURCEID
On/Off Switch This item is available when the Source is set to 0 - User. This applies voltage to or removes voltage from the IO pin. DOUT#.STATEU
LED icon This LED displays the state of the output, green for Active, off for Inactive. DOUT#.STATE

Bi-Directional I/O

The drive has a number of bi-directional I/O on the X22 and X23 connectors. DIO1-2 are on X22 and DIO3-6 are on X23. These can be used as general purpose I/O when the corresponding X22/X23.MODE keywords are set to GPIO (default). DIO#.DIR controls which direction that I/O will operate in. When configured as an input, the associated input keywords are available and the signal can be used for any input function. Likewise, when configured in the output direction, the associated output keywords are available and the signal can be used for any output function.


  • X22/X23 connectors and corresponding bi-directional I/O may not be available depending on the drive model being used.

Element Descripion Parameter
Direction

Set whether the I/O is used as an input or output.

  1. Input - this enables the Polarity and Filter settings.
  2. Output - this enables the Source and Source ID settings.
DIO#.DIR
Termination

Set whether the I/O is terminated or not.

  1. Not terminated
  2. Terminated
DIO#.TERM
Polarity

Set the polarity of the I/O when it is configured as an input,

  1. Active High
  2. Active Low
DIO#.INV
Filter

This item is available when the I/O is configured as an input. Setting a filter blocks input changes from registering until the specified pulse width is exceeded.

  1. Off (unfiltered)
  2. 10µs (fast)
  3. 163µs (standard)
  4. 2.62ms (slow)
  5. 240ns (ultra fast)
DIO#.FILTER
Source

Set the source of the I/O when it is configured as an output.

  1. User - the output value is controlled by the user.
  2. Action Table - the output value is controlled through the Action Table.
  3. Compare Engine - (Needs more info, not in the parameter description!)
DIO#.SOURCE
Source ID Sets the source ID of the selected source when required. In some cases, the source could have several instances and the user has to select which one to use. DIO#.SOURCEID

Related Topics

Action Table | Hardware Enable | Hardware Limit Switch | Capture